The fully automatic systems from Carl Cloos Schweißtechnik GmbH fulfil the highest safety requirements, which also apply to the energy supply systems used. In the application, these must move the cables and hoses for power, data, pneumatics and hydraulics in an upright, horizontal, suspended or linear sliding position without interruption. The special tandem arc process in particular required an energy chain that could easily cope with the additional loads from the cable and hose. The welding process was developed by Cloos in 1996. The technology involves two arcs burning in a common fusion strip. The result: the welding process is faster, the seams are longer and the deposition rate is higher. Overall, the additional cables and hoses achieve a weight of up to 10 kilograms per metre.
The machine manufacturer also required an energy chain solution for another system for the production of control cabinet frames whose length, width and height can vary greatly. The fully automated production system for welding the frames consists of 15 interlinked robots, a number of manipulators and extensive control technology that coordinates the production processes. Thanks to the use of a Cloos system and an extensive conversion, cycle times have been significantly improved and downtimes permanently reduced.