Change Language :

For unshielded chainflex® cables there is a tear strip under the outer jacket, for shielded chainflex® cables under the inner jacket. With just a few movements, the jacket can be opened to the desired length like a zip by simply pulling on the special tear strip. The outer jacket/inner jacket can then be removed from the core without risking damage to the core.
This not only saves installers and electricians time, but also additional tools. The cables are designed so that the cord does not cause any damage to the jacket or core even after millions of movement cycles.