Analysing technology

„SpeciMold“ from Brabender is an inline specimen-injection moulding system for recipe optimisation and quality assurance in the area plastic processing. The system subdivides into the heated SpeciMold blocks by piston and nozzle and a tool shape, which is opened and closed via a toggle lever mechanism. It is used in the classical compounding line between twin-screw extruder and nozzle head. The toggle lever mechanism corresponds primarily with the design of a conventional injection-moulding machine. The guides of the moved form plate as well as the support of the toggle lever are solved by igus® plain bearings from the drylin® R series: Four plain bearings are used in the executed version with lowered bearing clearance RJuM-12-30. The mechanics of the toggle lever is in addition supported by two press-fit bushes drylin® R-WLM. The stability of the process could only be reached with the use of these plain bearings. Besides solving the mechanical problems, a maintenance- and lubrication-free bearing is advantageous, especially for laboratory users.
Inline test specimen injection moulding system

Brabender GmbH & Co. KG, Stephan Mühlhausen, Duisburg, Germany

Here, you can find the products used

Here you can find further interesting applications from very different areas of use:

Go to manus® competition



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH