A new look at the origin of the universe

Researchers at the University of Lisbon use e-chains for a new type of multi-object spectrograph

gold vector

Profile

  • What was needed:  energy chain made of high-performance plastic from the triflex series ®
  • Requirements: The optical fibres of the spectrograph must only be exposed to low loads during movement. In addition, the guidance must function reliably under high ozone exposure.
  • Industry: Aviation technology
  • Success for the customer: The guidance system works so precisely and gently that it does not interfere with scientific observations. The solution is fail-safe even when ozone levels are permanently high.

Problem

Solution


igus® supported us in the initial search for a 3D solution and in obtaining information about the material properties to validate their application. This support was very useful to help with the final implementation of the solution.

Instituts für Astrophysik der Universität in Lissabon

Spectrograph of the University of Lisbon
energy chain from igus® in the spectrograph
energy chain from igus® in the spectrograph

ASI Automatikk AS Distributor+47 9006 1100