The product range of GROB-Werke GmbH & Co. KG includes flexible manufacturing systems for the automotive industry. These include machining centres, special machines and their automation.
The company has developed a new linear gantry, also known as a translator, which was presented with great success at the EMO.
The new linear gantry, or translator, is much more compact and smaller than the company's previous solutions. The height of the X-beam above the hall floor is just under 3.20 metres.
A new development is the vertical suspension of the carriage, which can carry loads of up to 80 kg, and the loading arm on large skate wheels below the X-beam. The already proven technology of the loading arm in parallel kinematics has also been further improved. The gripper can be supplemented by a swivelling axis in the A or C direction. By reducing the moving masses, significantly higher travelling speeds and acceleration values are achieved. With a travelling length of up to 40 m, the speed is 6 m/s and the acceleration 6 m/s2. Speed and acceleration were thus twice as fast as with the previous model. The significantly improved dynamics of the linear gantry enable the loading of interlinked single and twin-spindle machines with a single gripper.
A complete production line consists on the one hand of the linear gantry and on the other hand of single and twin-spindle machining centres for the workpieces.
Due to the high dynamics of the gantry, questions quickly arose for those responsible regarding the appropriate energy supply system. In addition to other requirements such as high wear resistance and a long service life, it was necessary for reasons of occupational safety that the sum of all noises should be relatively low at the same time.