Change Language :
The USB interface is emerging as one of the leading standard interfaces in digital camera technology. Responsible for the interference-free transmission of large amounts of data, it must be able to withstand mechanical load and the high electromagnetic compatibility requirements of the industry under all circumstances. For clean signal transmission, a camera manufacturer recommends its customers industrial USB cables, which can now be used up to a length of 10m.

Robust chainflex cables transmit data up to 10m. The camera manufacturer recommends the igus cables for industrial use.
"It's so easy!" is the corporate philosophy of IDS Imaging Development Systems GmbH, Obersulm." Our compact cameras are based on the central customer benefit of easy installation and simple use," explains Marketing Manager Thomas Schmidgall. "We pay attention to the highest quality. It starts with the development and ends with the accessories." For the cameras that are used in rough, industrial image processing, IDS offers its customers USB cables as accessories that have been specially developed by igus for high data transmission requirements. For dynamic movements in measurement and testing technology or for robot use, we recommend the industrial chainflex CFBUS.065 and CFBUS.066. "The robustness and signal quality convinced us right from the start," so Schmidgall. "Starting from a length of 5m, we only specify the industrial bus cables from igus for perfect data transmission. Conventional cables cannot withstand the mechanical and electrical loads over the long term." "We have spent a long time looking for ways to implement a transmission length of 10m for industrial use, so that no other fault-prone components come into play. Before we came across the chainflex cables, we tested a large number of cables from a wide variety of suppliers. None of them could withstand the requirements of interference-free signal transmission." The USB connection itself is not the problem, but the mechanical and electrical loads caused failures time and again.
In the visualisation, the demands on the functioning transmission of the data volume are exceptionally high. "The signal quality of the USB cables used is very good. We carried out a large number of comparison tests in advance; after a long search, the igus cables proved to be the right solution; they convinced us in terms of quality," concludes Thomas Schmidgall.
In person
Monday to Friday: 8 am – 8 pm
Saturday: 8 am – 12 pm
Chat-Service
Monday to Friday: 8 am – 4 pm
WhatsApp-Service
Monday to Friday: 8 am – 4 pm