The GES2 auditorium is a prestigious venue, for which an elaborate multimedia installation including a special cable winch construction was planned.fa The Italian specialist for stage and theatre technology, Alfa System Sas, was entrusted with the task of ensuring the complete installation and reliable moving of spotlights, projectors, loudspeakers and other stage elements.
The idea: several winches were to be arranged side by side in batteries, each moving a rod onto which the expensive equipment could be hooked. In the case of lights, projectors and loudspeakers, the power and control cables to these devices must also be guided safely.
As the GES2 auditorium is part of a very prestigious complex for hosting top-class events, the multimedia systems installed are all of excellent quality.
In addition to stringent requirements for cleaning the installation, there were therefore also strict regulations regarding the types of cables to be used and their performance. In addition, the cabling of the devices entailed high specifications with few possibilities for compromise. High-resolution cameras, speakers, microphones, light projectors and other devices all had their own cable requirements.