Change Language :

The tried-and-tested e-skin soft is now available in sizes 20, 24, 28.068 and 40 in dissipative material. This prevents the formation of electrostatic fields and the abrupt discharge caused by the movement of the black e-skin soft due to the material. The e-skin soft ESD is suitable for the highest cleanroom classes and requires very little installation space. It has a self-supporting function and a closed design.
There are two adversaries in modern battery production: moisture and contamination. Machines and systems must therefore function in extremely dry environments that have a relative humidity of less than 1%. They must not release any particles that could damage the sensitive cell materials. This also poses a challenge for energy chains that guide cables and hoses to moving machine parts, for example in cell assembly. Frictional conditions change in extreme dryness, which can increase wear and particle emissions. "For this demanding scenario, we have developed e-skin soft ESD systems. They are made of high-performance plastic that is particularly abrasion-resistant, so that virtually no particles are emitted even during fast movements in an extremely dry atmosphere," says Kira Weller, Product Manager for e-chains and cleanroom expert at igus. Proof is provided by a new certificate from the Fraunhofer IPA, according to which the e-skin soft ESD is the world's first energy chain in dry cleanrooms to achieve the highest degree, ISO Cleanroom Class 1. Weller: "The certificate is an important milestone for us. With the global expansion of battery production, the requirements for process reliability and purity are constantly increasing. We assume that industry and regulators will therefore demand even higher standards in future. Energy chains certified according to ISO 1 already provide the security for future high-purity production plants in the battery industry."
igus has been working with the Fraunhofer Institute for Manufacturing Engineering and Automation IPA for several years to have its energy chain systems independently tested and certified. However, specifically for dry cleanrooms testing technology previously set limits. In the past, certifications were only possible up to ISO Class 4 under dry cleanroom conditions. With a new test facility, the Fraunhofer IPA can now examine particle emission behaviour under dry cleanroom conditions up to ISO Class 1 for the first time. The results create additional transparency for users who have the highest requirements for cleanliness and process safety. Two designs for a wide variety of
Energy chains made of conductive ESD material are used to avoid static charge in manufacturing processes for electronic components or assemblies. Measurements of the electrical surface leakage resistance for igus® energy chains with the special material igumid® GC, were made back in 1992 by igus SE & Co. KG together with the PTB (Physikalisch-Technische-Bundesanstalt) in Braunschweig, supplemented by additional certifications in 1998 and 1999 according to DIN 53482, and the guidelines for static electricity ZH1/200 of the Federation of Trade Associations.

e-skin soft SKS | For unsupported lengths of up to 1.3m and installation space starting at 150mm