Change Language :
50% less installation time for the energy supply

The powerful "viapal" storage and retrieval unit from viastore systems, Stuttgart, can lift Euro pallets weighing up to 2,000kg. The device is 43 metres high and achieves an acceleration of up to 0.5m/s2 and travel speeds of up to 4m/s. The stroke acceleration is up to 1.5m/s2 and the stroke speed up to 1.33m/s.
The company was founded in 1988 within the C. Haushahn Group, but has been active in warehouse technology since 1970. With around 350 employees, viastore is one of the leading international suppliers of turnkey material handling systems for industry and trade. These include order picking systems, high-bay warehouses, automatic mini-load warehouses and complex distribution and logistics centres. The company plans and implements new systems as well as modernising existing warehouses and adapting them to the latest technologies and changing processes.
... and much more.

What our customers say
"We have been working together as partners for more than 15 years. So viastore, for instance, has been using pre-fitted energy supply systems for years, which are delivered directly to the machine on time. They are then simply assembled there," reports Wehrle.