Change Language :
The Waldbröl-Brenzingen wastewater treatment plant, which was built in early 1970 and significantly expanded in 1991, is one of 38 wastewater treatment plants operated by the Aggerverband in the Bergisches Land region. It treats the wastewater produced in large parts of the town of Waldbröl and is designed for 10,200 population equivalents. An energy supply solution now had to be found for the mobile scraper of a clarifier. The Aggerverband decided against the conventional solution with cable drum and in favour of an energy supply from the lbt flizz® system from igus®. The result: the system at the sewage treatment plant has been working without any failures since 2000.
The system has been running without any problems since it was installed in 2000. Maintenance costs have therefore been drastically reduced. It is therefore not surprising that the Aggerverband is satisfied with this solution. Those responsible also give the service from igus® good marks. Reinhard Braun, Head of Electrical Engineering at the Aggerverband, comments: "Our contacts have always responded quickly and unbureaucratically."
The lbt flizz® system has proven itself under adverse environmental conditions, and not only in this application. All the materials used in the system are corrosion-resistant and weatherproof. A correspondingly large number of other possibilities have already been realised, for example in rainwater overflow basins or harbour cranes, which have to meet extreme corrosion protection requirements. As the system components are also resistant to common chemicals, greases and solvents, igus® also supplies the lbt flizz® system to manufacturers and operators of galvanising plants and other chemical engineering facilities.
Here you can find the products used
You can find more interesting applications from a wide range of areas here