Change Language :
The strain relief of cables is a decisive factor for the safety, durability and reliability of energy supply systems in industrial applications. Particularly in dynamic environments, such as those found in automation technology and mechanical engineering, cables in energy chains are continuously exposed to mechanical loads.
This white paper sheds light on the technical importance of strain relief, presents various technologies and shows how strain relief can increase the operational safety and efficiency of industrial equipment.

A strain relief is a mechanical device that prevents tensile forces from acting uncontrolled on cable connections. A strain relief is particularly important in dynamic or heavily stressed applications to prevent damage such as cable breakage or vibrations and shocks.
The right strain relief offers several decisive benefits:
Increased service life of the cables: Reduction of mechanical stress and prevention of cable breaks
Greater operational reliability: Fewer breakdowns due to damaged cables
Economic efficiency: Fewer cable breaks and failures significantly reduce repair and maintenance costs
Better performance: Cables can work more trouble-free, even with long and intensive mechanical use
A cable feed-through with strain relief secures the cable in the cable gland or plug-in connector. The strain relief ensures that external forces are not transferred to the cables, but are absorbed by the structure on which the strain relief is assembled.
The forces at the contacts in the connector or in the cable are then close to zero. No matter how much the cable moves on the outside, it is at rest on the inside. This protects the contacts and sensitive electronics.
To ensure optimum energy chain performance, the following criteria should be taken into account:
igus has established itself as a leading supplier of energy chains and accessories and offers numerous unique selling points that play a decisive role in the choice of strain relief for cables in energy chains. Here are the main reasons why strain relief devices from igus are the better choice for many applications.

A series of in-house tests have shown that a small distance between the strain relief and the bend in the energy chain has no negative impact on the durability of chainflex cables. It is therefore possible to integrate a strain relief for cables directly into the mounting bracket. We offer strain relief options, e.g. the chainfix clamps or the space-saving tiewrap plates for almost all energy chains.
It is known that strain relief can considerably increase the service life of cables and hoses in energy chains. However, an incorrect strain relief can also have the opposite effect. For this reason, operators always ask themselves: should the strain relief be on one side or on both sides? The answer is simple: it depends on the application.
igus strain relief devices are tested under real-world conditions in the in-house igus laboratory, taking into account many different parameters, whether under the influence of fluids such as water or oil at various ambient temperatures. The interaction between strain relief devices and the different jacket materials of cables and hoses naturally also plays a role during in-house tests
The strain relief of cables is a decisive factor for the safety, durability and reliability of energy supply systems in industrial applications. Particularly in dynamic environments, such as those found in automation technology and mechanical engineering, cables in energy chains are continuously exposed to mechanical loads.
This white paper sheds light on the technical importance of strain relief, presents various technologies and shows how strain relief can increase the operational safety and efficiency of industrial equipment.