Change Language :
... and much more.

CNC (Computerised Numerical Control) machines have become indispensable in the industrial processing of materials. The use of computer technology in industrial processing not only increases precision and therefore manufacturing quality when processing workpieces, it also significantly increases productivity. CNC-supported machines are used today in a wide variety of applications. Our energy chains, linear guides and plain bearing systems are used in this selection of CNC milling, drilling, grinding, turning, cutting, polishing and bending machines.
Whether bending simple or complex parts, with TruBend machines from TRUMPF, a wide variety of workpieces can be bent quickly and reliably with maximum precision. For large and heavy parts, a bending aid supports the machining process. TRUMPF relies on our R4.1L series energy tubes to ensure the safe energy supply of this support.


15 e-chains are used in a milling machine in all travel axes, the lifting cabin and in the tool changer. They guarantee long travels of up to 50 metres.
To the application exampleAggressive ambient conditions usually occur when metal is being machined. Metallic grit, but also clogging oils for lubrication of machine parts, affect elements such as the cable guide or linear guide systems. Closed energy chains or energy tubes are often used to protect the internal cables in order to operate machines with as few interruptions and failures as possible.
Large machining centres in gantry design are the speciality of machine tool manufacturer Kao Ming from Taiwan. The long travels of up to 13 metres place special demands on the supply of energy and media in these systems. With the guidelok, Kao Ming has opted for a system that is reliable, robust and unsupported.

In the further development of machine tools, designers are looking for ways to reconcile ever more powerful systems with the endeavour to find space-saving solutions. This not only enables smaller dimensions for the entire system, but also offers considerable potential savings in terms of energy costs during operation. In this context, energy chain, for example, must allow very small bend radii at high travel speeds and accelerations.
The "System Technology" division of the renowned motorised spindle manufacturer FRANZ KESSLER develops and produces pivoting spindle heads and rotary pivoting tables, which enable a very precise processing of metal and increasingly also composite workpieces. For the power and signal supply, KESSLER uses chainflex cables that fulfil very high requirements in terms of service life and reliability.

When developing machine tools, a particular focus is placed on the high availability of the solution. The aim is to reduce downtimes and thus enable the customer to operate the machine as economically as possible. The high-quality systems often have to be able to cope with three-shift operations seven days a week without any problems. In the following application examples, the customer focussed on energy chains, linear guides or plain bearings that work reliably under the high and continuous stress from movement.
In hardly any other industry is reliability as important as in the automotive industry. Because production downtimes are expensive, it is important for vehicle manufacturers and suppliers to be able to rely on dependable components. An Austrian engine manufacturer therefore relies on 'smart plastics' from igus. Sensors detect wear during operation and raise the alarm in good time as soon as a repair or replacement is required.

Nowadays, modern machine tools can take several months from assembly to commissioning. However, in order to ensure ongoing operation at an earlier stage, highly complex systems should ideally be ready for operation after just a few weeks. Sophisticated modular products, expert advice and the reduction of the supplier base were able to contribute to this goal in the following applications.
The machine tool manufacturer Hartford from Taiwan relies on completely harnessed energy chain systems in its gantry machining centres. This saves many work steps, reducing the assembly time required from several weeks to just half a day. At the same time, customers can always rely on readychains to provide them with a reliable solution from a single source.


Trima Triebeser Maschinenbau GmbH has installed an e-chain with extender crossbars for the 300mm thick suction hose for a woodworking machine. The aim was to realise a cable-friendly and robust guide over a long travel.
To the application example