Change Language :
In cable trolleys, also known as cable trolleys, the cables hang unprotected from cranes in wind and weather. The cables themselves and the cable trolleys are exposed to fluctuating temperatures as well as sand and salt (in outdoor installations). Wind can easily cause the cables to become entangled, which can quickly lead to downtime. igus® offers a safe and modular alternative to cable trolleys on crane systems, which allows you to save cable length and avoid downtime. Energy, data, fibre optic cable, oil and air are safely routed in one system. More than 1,300 STS and over 6,500 RTG/RMG ASC cranes have been equipped with energy chain.
Free white paper:
plastic-energy chain in comparison to cable trolleys
In this white paper you can find the following topics:

We have compared energy chain systems and cable trolleys on a 100 m system:
The new heavy-duty roller chain fulfils all the requirements that apply to container cranes of the next generation and beyond.
Ever longer distances, higher dynamics, short load cycles, zero failures: That, in a nutshell, is what manufacturers of ship-to-shore container cranes demand for energy chain on crane bridges. The new P4HD.56R fulfils these requirements - with maximum cost-effectiveness.