Change Language :
The igus Robot Control makes it easy and intuitive to program, simulate and control robots. Its modular design supports a range of robot kinematics, including delta robots, gantry robots and multi-axis articulated robots. Individual robot movements and motion sequences can be tested in an integrated 3D simulation without connecting a physical robot. The robot programming software is available to download free of charge, with no licence fees or time limits.
Programming examples of various applications with the robot software
System requirements:
The PLC interface (PLC = Programmable Logic Controller) enables the execution of basic functions and the signalling of states by means of digital inputs and outputs. In addition to the control by a PLC, this interface also enables operation via hardware buttons.
Robot programs can be loaded and started and gripper commands can be sent via digital inputs or global signals. This is useful, for example, if a program is to be selected from a given selection using buttons or the CRI-GSig instruction.
The Modbus TCP interface can be used to send PLC data and instructions to the robot control system and receive status information, for example.
The CRI interface enables complex instructions to be sent and information and settings to be retrieved via the Ethernet interface using TCP/IP. The igus Robot Control uses this interface to connect to robots with an integrated control system or other instances of the control system.
The camera interface enables the use of object detection and video cameras. Object detection cameras recognise the position and class of objects and transmit these, optionally with a video image, to the control system. The control system calculates positions in the robot coordinate system from the object positions of the camera. Pure video cameras only deliver images and can therefore only be used to monitor the work area, but not to detect objects.
The Cloud interface enables the robot to be monitored via RobotDimension. Once activated and logged in, the robot sends basic status information and camera images to the online service. The user can list their robots on the website and retrieve the information.
Integrate the robots into your ROS environment. Documentation and packages for hardware communication, Teleop and moveI

The assembled tool can be specified here. Changing the tool requires the project to be reloaded or the integrated control system to be restarted. New tools can be defined as a configuration file in the directory "Data/Tools"

The range of movement of the robot arm is restricted by the settings of the virtual box. This functionality helps to prevent mechanical damage and simplifies programming, depending on the application. If a program is executed that violates the virtual box, it is stopped with an error message.

The robot control system supports up to 3 additional axes (also called "external axis" in iRC). These can be installed according to the robot axes and configured via the configuration area of iRC.

Here you can define the robot and logic program, the movement speed (as a percentage of the maximum speed), the playback mode and the reaction to program errors.

The robot control system can be customised for your robot with a digital twin. We configure the inverse kinematics to suit your project business.

The Joint command moves the robot to an absolute target position that is specified in axis coordinates (e.g. axis angle or position of a linear axis). The resulting movement of the TCP is usually a curve and not a straight line.

The Linear command moves the robot to an absolute target position specified in Cartesian coordinates. The resulting movement of the TCP follows a straight line.

The instruction "Circular movement" enables movements along a full or partial circular path. It is compatible with linear movements so that the transition from and to linear movements can be smoothed over.

Conditions can be used in if-then-else commands, loops and as cancellation conditions in motion commands. The conditions can be combinations of digital inputs, global signals, Boolean operations and comparisons.

The grid instructions calculate positions aligned to a grid, e.g. as a gripping or depositing position for palletising tasks.

The Relative command allows you to move the robot relative to its current position. It can be accessed via the menu items under "Action" → "Relative movement".

Sub-programs can be called up with the sub-command. The path to the sub-program file is specified under "File name". It is relative to the subfolder "Programs" of the iRC folder "Data".

Two types of variables are supported in the program for igus Robot Control and TinyCtrl:
The igus Robot Control software provides an intuitive environment for programming, simulating, and controlling different robot kinematics. For customized automation applications, developers can also connect the robot controller to external software through open interfaces. In particular, Python and C++ offer flexible options for developing custom functions and integrating robots into existing software and automation environments. [igus.de], [wiki.cpr-robots.com]
The App Interface provides an API and sample code for both Python and C++. Developers can use it to process robot controller status information, modify program variables, and implement custom functions for individual automation tasks. Since the interface is based on gRPC, additional programming languages can also be integrated with corresponding development effort.
For external robot control, developers can also use the CRI Ethernet Interface. This TCP-based protocol makes it possible to send robot motion commands, control digital outputs, modify variables, and load, start, stop, or monitor robot programs. A Python library is available to support the development of corresponding applications.
New robot applications can first be tested using the simulation provided by the igus Robot Control software. The same communication protocol can then be used with the physical robot by adjusting the IP address and port configuration. This allows developers to validate workflows before commissioning and reduces the effort involved in integrating the robot into the final automation system.
By combining an accessible graphical programming environment with the advanced capabilities of Python, C++, APIs, and open robot interfaces, igus Robot Control provides a flexible foundation for custom robotics solutions, external system integration, and the automation of complex processes.
The licence-free igus Robot Control software is integrated into the control system and therefore uses a standardised operating concept and consistent communication services for many components of one system. This means less project planning work and faster commissioning.

Robot programming software is an application used to program, simulate and control physical robots. Users can define motion sequences, move robots to specific positions, create robot programs and configure communication between the robot, controller and connected components. Common terms for this type of application include “robot control software”, “robot programming software” and “robotics software”. It is important to distinguish robot programming software from software robots. A software robot usually refers to an RPA bot that automates repetitive digital business processes in systems such as SAP, ERP or Microsoft Office. igus Robot Control is not an RPA solution. It is software designed for physical robot hardware and industrial automation applications
Many robot programming solutions are either time-limited trial versions that require payment after the trial period or proprietary applications that only work with robots from a single manufacturer. igus Robot Control is permanently free to use, with no licence fees or time limits. The software supports multiple robot kinematics and can be integrated into existing automation environments through open interfaces for ROS, MATLAB and LabVIEW. Users also benefit from free sample programs, comprehensive wiki documentation and practical robot programming training for beginners and advanced users.
The integrated 3D robot simulation environment allows you to plan and test motion sequences before connecting a physical robot. A digital twin provides a virtual representation of the selected robot kinematics. This offline robot programming functionality helps identify errors at an early stage and reduces commissioning time. Once the robot program has been tested in the simulation, it can be transferred directly to the physical robot hardware.
• Programming for delta, gantry, SCARA and articulated robots
• Intuitive 3D interface with a digital twin for robot simulation
• Linear, circular and axis-specific motion commands
• Conditions, loops and subroutines for complex automation sequences
• Virtual workspace limits and position variables
• Configuration of grippers and up to three external axes
• Camera and PLC interfaces for object detection and automation
• Communication via digital inputs and outputs, Modbus TCP/IP and CRI
• Integration with ROS, MATLAB and LabVIEW
To get started, you only need a computer running Windows 10 with approximately 500 MB of available storage space. An Ethernet or Wi-Fi connection is required to communicate with the robot.
For each project, users can configure grippers, virtual workspace limits, up to three external axes, individual error-handling settings and playback modes. The inverse kinematics can also be adapted for custom robot configurations. Available programming functions include axis movements in joint coordinates as well as linear and circular movements in Cartesian coordinates. Conditions, loops, subroutines and matrix calculations can be used to create complex programs and palletising applications. Relative movements based on the robot’s current position, numerical variables and position variables complete the range of programming functions.
igus Robot Control provides several interfaces for controlling robots during operation. These include PLC connectivity via digital inputs and outputs or Modbus TCP/IP, the CRI interface for sending complex commands over Ethernet, and a camera interface for object detection. The robot can also be monitored remotely using the RobotDimension cloud. These connectivity options allow the software to integrate directly into existing robot control and industrial automation environments rather than operating as an isolated system.
Pre-programmed sample projects for igus robots, individual axes and automated guided vehicles make it easier to get started. Comprehensive wiki documentation provides answers to detailed technical questions. Practical training courses for beginners and advanced users teach robot programming in either individual or group sessions.
igus Robot Control is available as a free download, with no licence fees, hidden costs or charges after a trial period. You do not need a connected robot to get started. Simply select the required robot kinematics, create a project and test your motion sequences in the integrated 3D robot simulation. Download igus Robot Control today and start programming, simulating and controlling robots for free