Individually adjustable lifting floors in floating systems

The dryspin lead screw technology enables the water level to be changed smoothly at the touch of a button

Changing the water depth at the touch of a button: Conmag Engineering GmbH from Austria builds adjustable lifting floors for swimming facilities with an integrated counter-current system. The aim is to keep the forces resulting from the water displacement as low as possible in order to ensure sustainable construction without endangering the stability of the system. In addition, the constant use under chlorine water places the highest quality demands on components and materials. As the entire mechanical system is located under water and is very difficult to access, all bearings must be maintenance-free and as low-wear as possible. 

Profile

  • What was needed: Plain bearings, linear guides, lead screws and lead screw nuts
  • Requirements: Chlorine resistance, weather resistance, low wear and maintenance, reliability and precision
  • Sector: Furniture construction & industrial design
  • Success for the customer: Savings of approx. €30,000 and 1kg of lubricant per system compared to previously used gearboxes. In addition, a flawless appearance of the luxury product is guaranteed.
Discover all of our products for machine tools
Swimming facility

Products used

Problem

The components of the lifting floors are constantly in contact with chlorinated water and must be weather-resistant. Since the entire mechanism is under water and is very difficult to access, all bearings must be maintenance-free and as low-wear as possible. Direct contact with the end user means that reliable as well as safe operation is essential to prevent injuries or damage to the system. As this is a luxury product, a flawless appearance also plays a decisive role. When lowering the lifting floor from the maximum vertical position, the aim is to minimise the forces resulting from water displacement in order to ensure a sustainable design without jeopardising the stability of the system. In addition, the constant use under chlorine water places the highest quality demands on components and materials. There are also numerous restrictions during installation due to work in the visible area or subsequent integration into existing systems.

Solution

Vertically adjustable lifting floors with thermal insulation effect for swimming pools: the aim of this development is to install vertically movable lifting floors in swimming facilities with integrated counter-current systems so that the pool depth can be individually adjusted. This makes it possible to use the pool surface as a terrace extension when raised and to adjust the water depth from a low height for non-swimmers to a depth of 1.5 metres as required. In addition, the lifting floor is fitted with 10cm of insulating material on the underside, thereby drastically minimising heat loss and the energy requirements of the system. In this task, which at first glance appears simple, constant compliance with the permissible gap dimension between the mobile floor unit and the stationary inner pool, which must not exceed 8mm, poses a special challenge when the pool size increases, as the water pressure increasingly deforms the pool walls, which are predominantly made of polypropylene. For this reason, the core competence to be developed is to design a linear movement of the lifting floor that is as continuous, precise and particularly reliable as possible  .

Swimming facility
Swimming facility
Lead screw technology in swimming pool
Lead screw technology in swimming pool
"Thanks to the igus components used, costs of around EUR 30,000 per system could be saved compared to the previously used gearboxes. In addition, lubricant consumption was reduced by approx. 1kg per year per system."

Overview of dryspin lead screw technology

Our advantages at a glance

  • Lubrication and maintenance-free
  • Higher efficiency
  • Longer service life thanks to asymmetry
  • Media-resistant
  • Quiet and vibration dampening due to thread geometry
  • Calculate service life online
  • Various materials and types
Holding a real sample in your hands is an important part of understanding your component. We would be happy to send you one. Individual samples can also be easily created. Get in touch with us.
 
Free sample enquiry



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH