Change Language :
Revolutionary system for the automation of offshore oil exploration in the face of extreme conditions
Metre-high waves, storms with high wind speeds, plus oil, mud and heavy rainfall: Living and working on an oil platform is not only uncomfortable, it is also dangerous. Drilling rods are driven up out of the borehole and unscrewed and reassembled by oil-smeared men under high pressure. A lot of manual labour under time pressure, in the dirt and with a high risk of injury. But all that could soon be over. The Norwegian company Robotic Drilling Systems has spent many years of research and development work developing a robotic system to automate the drilling processes on the platform. energy chains from igus® ensure a reliable energy supply under extreme conditions.
"It is important for us to obtain components for the robots from a single source and, if possible, ready to install. The systems should also be as maintenance-free as possible. This can be guaranteed by igus®."
Jimmy Bostron, Chief Operating Officer of Robotic Drilling Systems
The robotic system developed by RDS is suitable for installation on new oil drilling platforms, but also for retrofitting. It creates new rules for assessing the profitability of exploration projects - an important factor in view of the low oil prices. For this reason, the new development met with great interest right from the start - and led, among other things, to well-known drilling companies participating in RDS. The jury of the vector awards initiated by igus® was also impressed by the application and honoured the system with the golden vector 2016 award. After extensive testing, the first practical installation was put into operation on an oil drilling platform in Norway in September 2015 (Fig. 5). The entire industry is closely following the project, which is making work on oil drilling platforms faster, cheaper and, above all, safer.
In person
Monday to Friday: 8 am – 8 pm
Saturday: 8 am – 12 pm
Chat-Service
Monday to Friday: 8 am – 4 pm
WhatsApp-Service
Monday to Friday: 8 am – 4 pm