Change Language :

Defining data volumes correctly for Ethernet cables
It is common practice to use the Ethernet cable with the highest possible category. However, this often means a high price and is not always necessary from a technical point of view. With this event, we want to convey an idea that choosing the right data transmission volume for cable can be a good option for saving money.
With the world's largest portfolio of Ethernet cables for motion, igus offers its customers the right choice for every application. Increasing automation in production is also increasing the amount of data that needs to be transmitted between individual components. At the same time, there is more and more movement in modern production processes, which is why cables specially designed for these purposes should be used. As the requirements for cables differ from application to application, we offer a complete product range of Ethernet cables specifically for motion. Depending on the required mechanical and electrical performance, users can rely on safe and tested cables and choose the most favourable cable from our range that is sure to work for them. From CAT5 to CAT7 transmission standards as well as simple linear or complex three-dimensional movement. Even applications with particularly high tensile forces can be realised - so we offer a suitable Ethernet cable for almost every application.

As it is not only the right cable that is important for the dimensions, but also the right connector, we work intensively with leading connector manufacturers to match connector and cable precisely. This provides security and also great advantages in terms of fit.
Example of long-term test 5006a of an Ethernet cable of the CFBUS series, with a test bending factor of only 9.8xd.