Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.
My contact person
ASI Automatikk AS

Distributor

Sankt Hallvards vei 3, port 8

3414 Lierstranda

NORWAY

+47 9006 1100
NO(EN)

Individual harvesting robot for strawberries: build or buy your robot

  • What was needed: tailor-made harvesting robot for strawberries
  • Requirements: fast ROI, weatherproof and modular components
  • Material: iglidur J2 plain bearings, drygear Apiro gear, drylin WSQ double rail
  • Industry: agricultural engineering
  • Success for the customer: greatly reduced costs, relief for employees, simple harvest planning


     
Request individual consultation now
Strawberry harvest with robot

About the application:

AINAC Systems Co. is currently developing an automatic strawberry harvesting system. For this purpose, a simple robot arm is specially developed which can pick strawberries with 3 axes (horizontal, vertical and rotation) without using an expensive articulated arm robot. Lubrication-free igus materials and modular gearboxes from the Apiro gearbox modular system are used for the main part of the robot structure.

The problem

The challenge in this application is to be able to work without problems in the humid environment of a plastic house, with water, mud and high humidity. The company had opted for plastic components in order to keep the weight of the Ernet robot as low as possible.

The solution:

For the construction of the harvesting robot, the company had initially considered worm gear units from other manufacturers. However, after receiving an Apiro sample box, Mr. Shigenori Inami was convinced that the Apiro modular gearboxes met his exact requirements.
The arm pivot bearings of the steering axle consist of the lubrication-free iglidur J2 material. Apiro gearboxes with optional shaft were used for the reduction gearbox for the wheel drive, steering and arm swing.
The horizontal and vertical arm movement mechanism consists of a drylin W double rail WSQ and a pillow block bearing.
With the igus modular system, the company AINAC Systems can build a custom, weather-resistant robot solution that is durable and safe despite low costs.


The terms "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "RCYL", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" and "yes" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries. This is a non-exhaustive list of trademarks (e.g. pending trademark applications or registered trademarks) of igus SE & Co. KG or affiliated companies of igus in Germany, the European Union, the USA and/or other countries or jurisdictions.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® SE & Co. KG